Search FAQs
What is the Anti-Jam function on the Altivar 6xx Process drive?
Issue:
Anti-Jam function on the Altivar 6xx Process drive.
Product Line:
ATV6xx
Environment:
All serial numbers for ATV6xx
Cause:
N/A
Resolution:
Clogging substances can damage the pump.
This function allows manually or automatically executing forward & reverse pump rotations cycles to unclog.
It may also help to clear a blocked impeller, pipe, or valve at downstream location.
This should increase he efficiency of the system as well as the pump life time.
Anti-Jam function on the Altivar 6xx Process drive.
Product Line:
ATV6xx
Environment:
All serial numbers for ATV6xx
Cause:
N/A
Resolution:
Clogging substances can damage the pump.
This function allows manually or automatically executing forward & reverse pump rotations cycles to unclog.
It may also help to clear a blocked impeller, pipe, or valve at downstream location.
This should increase he efficiency of the system as well as the pump life time.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: