{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is Macro Configuration on the Altivar 6xx Process Drive?
Issue:
Macro Configuration on the Altivar 6xx Process Drive.

Product Line:
Altivar 6xx Process Drive

Environment:
All serial numbers for Altivar 600 Process Drive

Cause:
N/A

Resolution:
[Complete settings] [Macro configuration]

This menu allows to select an application type
●The target is to display only parameters and menus useful for the selected application.
●The application type selection should be done prior to the application settings
●Partial factory settings in case of modification.

●Applications available are:
- Generic Pump Control (default fault setting)
For Generic Pump Function controls like PID regulator, Sleep Wake Up, etc...

- Pump Level Control
Turns on Level Control functions - [Complete settings] [Pump functions] [Level control]
The aim of the level control function is to operate:
Filling operation
Emptying operation
This function offers a random level functionality by changing the start and stop level after each operation
(at the end of filling or emptying operation) in order to start and stop the next filling or emptying operation
from different levels.
The level control function can be used for single pump or multi-pump architecture.

- Pump Booster Control
Turns on Booster Control functions - [Complete settings] [Pump functions] [Booster control]
The aim of the booster control function is to maintain the desired pressure at the outlet of the pumps
according to the demand by:
Managing the velocity of the variable speed pump connected to the drive.
Staging/De-staging the auxiliary fixed speed pumps

- Generic Fan Control
Turns on Fan Control functions - [Complete settings] [Fan]
For Generic Fan Control functions like Fan PID controller, feedback, etc...

Schneider Electric Nigeria

Attachment(s)
ATV6xx_Programming_Manual_EN_EAV64318_03 (Macro-Config).pdf [55.62 KB]