{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the standard overload range for form H30 on an 8536 type S starter?

Issue:
SSOLR code for 8536 type S Starter

Product Line:
NEMA Type S starters

Environment:
Type S Full Voltage Contactors and Starters

Resolutions:
The standard overload range will depend on the starter size.  Note the range can be changed.  Check the Digest for details on modifying the form.
Size0001234567
(SSOLR comes standard)
Amp Range3-96-189-2715-4530-9045-13590-270180-540270-810

Schneider Electric Nigeria