{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between the AS-MBKT-085 and the AS-MBKT-185 Modbus Plus connectors?
Title
Difference between the AS-MBKT-085 and the AS-MBKT-185

Issue
Modbus Plus Connector difference

Product Line
Modbus Plus

Resolution
The AS-MBKT-185 connector has an integrated 120 ohm terminating resistor. These connectors can only be installed on the ends of the Modbus Plus network. The AS-MBKT-085 connector does not have an internal terminating resistor. These connectors can be installed on any Modbus Plus node in between the end nodes. The AS-MBKT -085 connector is a dark gray color whereas the AS-MBKT -185 connector is a light gray color..

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria