Issue:
Is there an EDS file available for the M221 Ethernet/IP communications?
Product Line:
TM221
Resolution:
Yes, the EDS file for the M221 is located in the installation path of Somachine Basic \Firmwares & PostConfiguration\M221
Please note that EDS file will need to be modified to match your settings in the Somachine Basic for Ethernet/IP configuration.
Attached is the EDS file and the instructions to modify the EDS file.
Is there an EDS file available for the M221 Ethernet/IP communications?
Product Line:
TM221
Resolution:
Yes, the EDS file for the M221 is located in the installation path of Somachine Basic \Firmwares & PostConfiguration\M221
Please note that EDS file will need to be modified to match your settings in the Somachine Basic for Ethernet/IP configuration.
Attached is the EDS file and the instructions to modify the EDS file.
Released for:Schneider Electric Nigeria