{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the power connector for the Magelis HMIGTO?
Issue
What is the part number for the power connector for the Magelis HMIGTO?

Product Line
Magelis HMIGTO

Environment
Physical HMI

Resolution
There are two different types of 3-pin 24VDC power connectors for the Magelis HMIGTO series.

Straight 3-pin 24VDC connector:
HMIZGPWS

Right-angled 3-pin 24VDC connector:
HMIZGPWS2

Both orders come with 5 connectors in the box.

A diagram of both can be found on page 70 of the product manual for the Magelis iDisplay which shares this power connector:
"Magelis iDisplay HMI DID, User Manual"
https://www.se.com/ww/en/download/document/EIO0000002044/

Schneider Electric Nigeria