The PNETR6 and the PNET1GB are compatible with the associated data rates of VDSL and connection of most modems. For applications requiring data line surge suppression for VDSL networks, either of these two models should be recommended, depending whether the application requires rack-mount or standalone installation.
Released for:Schneider Electric Nigeria
The PNETR6 and the PNET1GB are compatible with the associated data rates of VDSL and connection of most modems. For applications requiring data line surge suppression for VDSL networks, either of these two models should be recommended, depending whether the application requires rack-mount or standalone installation.