{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What wires are protected by the various ProtectNet models?
PNET1GB and PNETR6 both protect wires 1-8 on an RJ45 cable
PTEL2 and PTEL2R both protect wires 1-4 on an RJ11-, or wires 3-6 on an RJ45 cable
PDIGTR protects wires 1-8 on an RJ45 cable
PS9-DCE and PS9-DTE both protect wires 1-9 on a DB9-RS232 cable

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.