{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the main function for the External Neutral Current Transformer (ENCT) that is used with NSX MCCB?

The external transformer is a sensor required for a three-pole circuit breaker in a

system with a distributed neutral to measure the neutral current in order to:

protect the neutral conductor

protect against insulation faults.

This current transformer can be connected to Micrologic 5 / 6 trip units. The transformer rating must be compatible with that of the circuit breaker.

Schneider Electric Nigeria