- For the Source change over system using MCCB of type NSX, in order to perform Load shedding and re-connection of on non priority loads,
This function is supported when using the Controller UA while it is not supported in the BA controller
This function is supported when using the Controller UA while it is not supported in the BA controller