{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Function of the interphase Barriers that are installed with NSX MCCB?

Safety accessories for maximum insulation at the power-connection points:

bb they clip easily onto the circuit breaker

bbsingle version for fixed devices and adapters on plug-in bases

bbnot compatible with terminal shields

bb the adapter for the plug-in base is required for mounting on plug-in and

withdrawable versions.

Schneider Electric Nigeria