{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the different ethernet racks available in M580 range ?
Issue:
What are the different ethernet racks available in M580 range ?

Product Line:
M580

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
M580 Ethernet racks have all the features of the X Bus racks with the addition of an Ethernet communication bus across the backplane.​

M580 Ethernet racks

All Ethernet racks are available in standard or industrially hardened versions. A hardened version has the letter H appended to the reference.

Schneider Electric Nigeria