Issue:
Loaded the EDS file for XPSMCMCO0000EI Ethernet IP but getting an error Incorrect Vendor Data. How to resolve the issue?
Product Line:
XPSMCM, SoSafe
Resolution:
This is a known issue, please see page 8 of attached document.
From that document: In the new XPSMCMCO0000EI firmware V1.8 version for the Vendor data contents have been updated. The previous EDS - files are not in accordance with the new data. This incompatibility appears also in combination of latest EDS file with EIP communication modules having previous FW version. As a result, during setup of the communication, it is not allowed to use the feature "Electronic Keying" (Vendor data checking).To enable the communication with EIP communication module FW V1.8 it is mandatory to remove ticks from "Electronic Keying" check boxes until EDS -file SE_ET_XPSMCM_0108E_20150916.eds in XPSMCM_Ethernet_EDS_V1_8_20150916.zip.
Loaded the EDS file for XPSMCMCO0000EI Ethernet IP but getting an error Incorrect Vendor Data. How to resolve the issue?
Product Line:
XPSMCM, SoSafe
Resolution:
This is a known issue, please see page 8 of attached document.
From that document: In the new XPSMCMCO0000EI firmware V1.8 version for the Vendor data contents have been updated. The previous EDS - files are not in accordance with the new data. This incompatibility appears also in combination of latest EDS file with EIP communication modules having previous FW version. As a result, during setup of the communication, it is not allowed to use the feature "Electronic Keying" (Vendor data checking).To enable the communication with EIP communication module FW V1.8 it is mandatory to remove ticks from "Electronic Keying" check boxes until EDS -file SE_ET_XPSMCM_0108E_20150916.eds in XPSMCM_Ethernet_EDS_V1_8_20150916.zip.