Search FAQs
In Dc cubicle of BlokSeT, is it possible to change Vertical Busbars by Cables?
We do not recommend to replace Vertical busbars by cables in case of Dc cubicles.
In Dc cubicles, the incoming connection to the circuit breaker for each capacitor steps / Functional units are tapped from the vertical busbars. If we remove the VBB, then we have to connect all the cables directly to the HBB. It is very difficult to control the cable bending angle and the cable may not be well supported.
Contact L3 support in case of any doubt.
In Dc cubicles, the incoming connection to the circuit breaker for each capacitor steps / Functional units are tapped from the vertical busbars. If we remove the VBB, then we have to connect all the cables directly to the HBB. It is very difficult to control the cable bending angle and the cable may not be well supported.
Contact L3 support in case of any doubt.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: