{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a way in Sepam 40 to know the status of the breaker via communication?
A MES module is needed to read the status of the breaker and then the “circuit breaker control” function should be activated. Input I11 is used to monitor the open position while input I12 monitors the closed position. Then read the input via Modbus communication.

Schneider Electric Nigeria