{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it okay to remove the front bottom conduit kit cover for the Altivar Process 600 and 900 Drives?
Issue:
Remove front bottom conduit kit cover for the Altivar Process Drive.

Product Line:
Altivar Process Drive

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
The Altivar Process drives are designed to have IP21 ratings which requires the control terminals and wires be finger safe.
By removing the front bottom cover those terminals become exposed as a result the drive will loose its IP21 ratings.

Schneider Electric Nigeria