{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Proper use of a "Make Before Break" bypass panel with an SURT or SRT UPS
Failure to follow the below instructions may result in the following fault messages on the SmartUPS:
P.11, SRT DC Bus Overvoltage, Event 118, Event 119, failure bypass

IMG1 IMG1 IMG1 IMG1

When moving from Normal to Test mode:

●Place UPS into internal Bypass
●Confirm UPS is in Bypass
●It is now safe to move the SBP to Test mode

When moving from Test to Bypass or vice versa:
●UPS can be in any state

When moving from Test back to Normal:

Place UPS into internal Bypass
●Confirm that UPS is in Bypass
●Move SBP to Normal
●Confirm UPS has no faults and input is acceptable to bring online.
●Take UPS out of internal Bypass

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: