Search FAQs
What are some of the benefits to the reduction of noise voltages with the Altivar 680/980 Series Variable Frequency Drives?
Issue:
Benefits to the reducing noise voltages with the ATV680/980 drives.
Product Line:
ATV680 ATV980
Environment:
All
Cause:
Benefits of voltage noise
Resolution:
The connection of DC-voltage midpoint with artificial star-point built by filter capacitors will reduce the bearing currents, increasing the lifetime of motor bearings and allows for easy paralleling of power stages.
Benefits to the reducing noise voltages with the ATV680/980 drives.
Product Line:
ATV680 ATV980
Environment:
All
Cause:
Benefits of voltage noise
Resolution:
The connection of DC-voltage midpoint with artificial star-point built by filter capacitors will reduce the bearing currents, increasing the lifetime of motor bearings and allows for easy paralleling of power stages.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: