{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

UL Certificate of Conformity for Harmony HMIGTO series HMI

Issue
Where do I find the UL Certificate of Conformity for Harmony HMIGTO targets and which UL enclosure types are they rated for?

Product Line
Harmony HMIGTO

Environment
Physical characteristics

Resolution
Attached is the UL Certificate of Conformity for Harmony HMIGTO targets.

The HMIGTO series is was tested for UL Enclosure requirements:
Type 1, Type 4X (Indoor use only), and/or Type 13 rated enclosures

Schneider Electric Nigeria

Attachment(s)

CoC MPCKT-HMIGTO_20140318-E194434 (new UL File No. E220851).pdfCoC MPCKT-HMIGTO_20140318-E194434 (new UL File No. E220851).pdf [267.51 KB]