{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I get a copy of the installation manual for the Altivar 930 and Altivar 950 Process Drive?
Issue:
ATV930/ATV950 Installation Manual request

Product Line:
Altivar Process Drive (ATV930, ATV950)

Environment:
All serial numbers for Altivar Process Drive

Cause:
Need to get more detailed information on:
Basic Drive Installation
Wiring Diagram
Drive Mounting
Drive Wiring
Dimensions
Temperature Conditions
Altitude Conditions
Derivative Curves
Power or Heat Dissipation
Operation on an IT or Corner Grounded System
Power and Control Terminals

Resolution:
ATV930, ATV950 Installation Manual
http://www.altivardrives.com

Schneider Electric Nigeria