{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV12 local operation Can the drive be programmed to restart after a power loss or power cycle local mode control?
Issue:
Can the Altivar drive be programmed to restart after a power loss?

Product Line:
All Altivar 12 drives

Environment:
All

Cause:
Power loss in local mode.

Resolution:
No, if power is loss in local mode control the run command is also loss and will require a restart command.

Schneider Electric Nigeria