{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Sepam ECI850 - how to check if the downstream Sepam relays on the RS-485 network have been disconnected?

For the Sepam ECI850 server, you can read the PhyHealth status value in the LPHD class.

If the Sepam devices defined in the ECI850 CID file have been disconnected from the RS-485 port and the number of retries has been exhausted, then this PhyHealth status will indicate a partial fault.

It is possible to add this data to a Dataset so that a Report could be generated from the ECI850 should the downstream Sepam devices become disconnected.

AEDL3

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.