{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What can't I load an application to an XBTGK2330 via an SD card?

If you get this error while updating the application with an SD card on a Magelis XBTGK2330:
“Upgrading BSP – the auto-installer has detected an error; your application might not function correctly. Make sure target type is correct”.

For the XBTGK2330 with DOM after 1523 you must use Vijeo Designer V6.2 SP3.1 or higher on the initial download

Schneider Electric Nigeria