{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How quiet (or noisy) is the NetShelter CX when only the fans are running, with no equipment installed?

Issue:
The question was raised asking how quiet the cabinet is with nothing installed, just the fans running.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Noise reduction in the office is important.

Resolution:

Noise of AR4018A / AR4018IA:
40.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet

Noise of AR4024A / AR4024IA:
43.0 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet

Noise of AR4038A / AR4838IA:
43.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet

Schneider Electric Nigeria