Issue:
Set up a 4-20mA Analog Signal on Altivar Process Drives.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
Altivar Process Drive
Resolution:
Wiring:
For wiring use AI3 and COM (AI3 is set to 4-20ma by default from the factory)
Can use the other analog inputs terminals on the drive as well (AI1, AI2, AI4, ...)
Setup:
[Complete settings] [Input/Output] [AI/AQ]
Set up a 4-20mA Analog Signal on Altivar Process Drives.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
Altivar Process Drive
Resolution:
Wiring:
For wiring use AI3 and COM (AI3 is set to 4-20ma by default from the factory)
Can use the other analog inputs terminals on the drive as well (AI1, AI2, AI4, ...)
Setup:
[Complete settings] [Input/Output] [AI/AQ]
Released for:Schneider Electric Nigeria
Issue:
Set up a 4-20mA Analog Signal on Altivar Process Drives.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
Altivar Process Drive
Resolution:
Wiring:
For wiring use AI3 and COM (AI3 is set to 4-20ma by default from the factory)
Can use the other analog inputs terminals on the drive as well (AI1, AI2, AI4, ...)
Setup:
[Complete settings] [Input/Output] [AI/AQ]
Set up a 4-20mA Analog Signal on Altivar Process Drives.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
Altivar Process Drive
Resolution:
Wiring:
For wiring use AI3 and COM (AI3 is set to 4-20ma by default from the factory)
Can use the other analog inputs terminals on the drive as well (AI1, AI2, AI4, ...)
Setup:
[Complete settings] [Input/Output] [AI/AQ]
Released for:Schneider Electric Nigeria