Issue:
Part number for the Apogee P1 option card for the Process drive
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Attempting to add the ATV630 to a Apogee network.
Resolution:
There is currently not a Apogee P1 option for the ATV630 or ATV930 process drives. Consider using a 3rd party's gateway to an embedded protocol.
Part number for the Apogee P1 option card for the Process drive
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Attempting to add the ATV630 to a Apogee network.
Resolution:
There is currently not a Apogee P1 option for the ATV630 or ATV930 process drives. Consider using a 3rd party's gateway to an embedded protocol.
Released for:Schneider Electric Nigeria