{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What parameters can be added to the ATV630 MyMenu?
Issue:
Needs to add parameters to MyMenu on an ATV630.

Product line:
ATV630, ATV600, Altivar Process

Environment:
all

Cause:
n/a

Resolution:
The MyMenu can only add parameters listed under the Complete Settings menu.  Other parameters, such as Motor Thermal State (THR) under the Display menu, cannot be added to the MyMenu.

Schneider Electric Nigeria