{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause you not to be able to change motor data settings in the ATV320 drives?
Issue:
Not being able to change motor data settings in the ATV320

Product Line:
Altivar 320

Environment:
All

Cause:
Function blocks are running the back ground you will need to stop the function blocks.

Resolution:
FbM- [FUNCTION BLOCKS] (continued)
FbCd

[FB Command]
Allows to start and stop the function blocks manually.
StOP
Strt
[FB Command] (FbCd) is forced to [Stop] (StOP) if there is no valid function blocks application in the drive memory.
[FB Command] (FbCd) is set to [Start] (Strt) when the function blocks application switch to Run according to
[FB start mode] (FbrM) configuration.
Note: As soon as the function blocks are started, the drive is considered as in running state and the modification of configuration
parameters is no longer possible.
[Stop] (StOP): Function blocks application Stop command
[Start] (Strt): Function blocks application Start command

Schneider Electric Nigeria