{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How is PID programmed on the ATV320 drives?

Article available in these languages: Dutch

Issue:
ATV320 PID set up.

Product line:
ATV320, Altivar 320

Environment:
all

Cause:
To maintain pressure, temperature or flow within a system

Resolution:
Using the dial on the display, Push Enter and turn to CONF > FULL > FUN > PID.

Under the PID Regulator menu set:
PIF - PID feedback assignment

PIF1 - Min PID feedback
PIF2 - Max PID feedback
PIP1 - Min PID reference
PIP2 - Max PID reference
PII - Act. Internal PID ref
RPI - Internal PID ref


Min/Max PID Reference and Feedback are typically set to the range of the transducer.  Act. Internal PID turns on the internal set point.  Internal PID ref is the set point you want to maintain.

Example:
You have a transducer, 4-20 mA output with a 0-100PSI range wired to AI3 and COM.  You want to maintain 40PSI pressure.  The recommended settings would be:
PIF - AI3
PIF1 - 0
PIF2 - 100
PIP1 - 0
PIP2 - 100
PII - yes
RPI - 40

This would maintain 40PSI (10.4 mA feedback) in the system based on 4-20 mA signal coming into AI3.
Feedback < 10.4 mA will increase motor speed.
Feedback > DVD will decrease motor speed.
If the VFD reaction needs to be reversed, set PiC, PID correct reverse, to YES.

RPG: PID Proportional gain and RIG: PID controller integral gain will usually need adjustment to limit overshoot and to stablize the response to system changes.  For most pump and fan applications, settings less than 1 provide acceptable response and the RDG: PID derivative gain can be left at 0.
If RPG is too high the system will overshoot the setpoint and can have significant instability before approaching the setpoint.
If RPG is too low the system may never reach it's setpoint.
If RIG is too high the system will search or hunt around the setpoint, taking a long time to stabilize.
If RIG is too low the system will take a long time to reach setpoint.
d

This is where you'll find the settings in SoMove:
d


The full ATV320 Programming Manual can found here: https://www.se.com/us/en/download/document/NVE41295/

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: