{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How to reset the Vijeo Designer layout back to default?

Issue:
Looking for a way to reset my Vijeo Designer windows. The Windows are all scattered.

Product Line:
Vijeo Designer (all versions)

Resolution:
Sometimes when you move the windows and panes around in Vijeo Designer, you may want to move them back to default. The easiest way to do so is with the following procedure:

Simply shutdown Vijeo Designer, open up REGEDIT and delete the following key:
-For Vijeo Designer v6.2 SP8 or older, delete:
HKEY_CURRENT_USER\Software\Schneider Electric\Vijeo-Designer62

-For Vijeo Designer v6.2 SP9 or newer, delete:
HKEY_CURRENT_USER\Software\Schneider Electric\Vijeo-Designer62B

After you delete that, restart Vijeo Designer.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: