{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to setup Limit Switches and Position Sensors on the Altivar 900 Process Drive.
Issue:
Set up Limit Switches and Position Sensors on the Altivar 900 Process Drives.

Product Line:
Altivar 900 Process Drive (ATV930, ATV950, ATV960, ATV980)

Environment:
All serial numbers for Altivar 900 Process Drive

Cause:
N/A

Resolution:
Limit Switches
This function allows the management of trajectory limits using limit switches
The stop mode is configurable. When the stop contact is activated, startup in the other direction is authorized.
Works best with Forward and Reverse Limit Switches.

Programming
[Complete settings] [Generic functions] [Limit switches]
Setup:
  1. [Stop FW assign] LAF
  2. [Stop RV assign] LAr
  3. [Stop type] LAS
Refer to attached manual for more information

Positioning by Sensors
This function allows the management of slowing down of movement and stopping at the end of a trajectory using positioning sensors.
Sensors are used to slow down the object in reverse or forward direction
Works similar to Limit Switches but also allows user to configure speed as well as stopping

Programming
[Complete settings] [Generic functions] [Positioning by sensors]
Setup:
  1. [Stop FW limit sw.] SAF
  2. [Stop RV limit sw.] SAr
  3. [Forward Slowdown] dAF
  4. [Reverse Slowdown] dAr
  5. [Disable limit sw.] CLS
  6. [Stop type] PAS
  7. [Deceleration type] dSF
  8. [Stop distance] Std
  9. [Nom linear speed] nLS
  10. [Stop corrector] SFd
  11. [Memo Stop] MStP
  12. [Priority restart] PrSt
Reference attached manual for more information


Key Notes:
If the drive is configured for limit switches/positioning by sensors the sequence of operation has to be correct or else the drive will not function properly.
Drive may show "rdy" at times even though a run command is initiated on LI1
Look at the example table below


For instance, SAF = DI5 and SAL = High
DI1 (forward)DI2 (reverse)DI5 (FW limit switch)Note
100Motor is running forward
101Motor is stopping
001Sensor stays at high level
011Motor is running reverse
010Motor is running reverse
000Motor is stopping
100Motor is running forward

Now if you do the sequence below the drive will stay in ready:
DI1 (forward)DI2 (reverse)DI5 (FW limit switch)Note
100Motor is running forward
101Motor is stopping
000Sensor goes back to low level
010Motor is running reverse
000Motor is stopping
100Drive stays in ready

The drive stays in ready as the behavior isn't coherent. The limit switch shouldn't have change of state, before reverse order.


Schneider Electric Nigeria

Attachment(s)
_9xx_20160921-Postioning by Sensors.pdf [120.4 KB]
ProgManual-Limit Switches and Positioning by Sensors.pdf [369.97 KB]
How to setup Limit Switches and Position Sensors on the Altivar 900 Process Drive.
Issue:
Set up Limit Switches and Position Sensors on the Altivar 900 Process Drives.

Product Line:
Altivar 900 Process Drive (ATV930, ATV950, ATV960, ATV980)

Environment:
All serial numbers for Altivar 900 Process Drive

Cause:
N/A

Resolution:
Limit Switches 
This function allows the management of trajectory limits using limit switches
The stop mode is configurable. When the stop contact is activated, startup in the other direction is authorized. 
Works best with Forward and Reverse Limit Switches.

Programming
[Complete settings] [Generic functions] [Limit switches]
Setup:
  1. [Stop FW assign] LAF
  2. [Stop RV assign] LAr
  3. [Stop type] LAS
Refer to attached manual for more information

Positioning by Sensors
This function allows the management of slowing down of movement and stopping at the end of a trajectory using positioning sensors.
Sensors are used to slow down the object in reverse or forward direction
Works similar to Limit Switches but also allows user to configure speed as well as stopping

Programming
[Complete settings] [Generic functions] [Positioning by sensors]
Setup:
  1. [Stop FW limit sw.] SAF
  2. [Stop RV limit sw.] SAr
  3. [Forward Slowdown] dAF
  4. [Reverse Slowdown] dAr
  5. [Disable limit sw.] CLS
  6. [Stop type] PAS
  7. [Deceleration type] dSF
  8. [Stop distance] Std
  9. [Nom linear speed] nLS
  10. [Stop corrector] SFd
  11. [Memo Stop] MStP
  12. [Priority restart] PrSt
Reference attached manual for more information


Key Notes:
If the drive is configured for limit switches/positioning by sensors the sequence of operation has to be correct or else the drive will not function properly. 
Drive may show "rdy" at times even though a run command is initiated on LI1 
Look at the example table below


For instance, SAF = DI5 and SAL = High
DI1 (forward)DI2 (reverse)DI5 (FW limit switch)Note
100Motor is running forward
101Motor is stopping
001Sensor stays at high level
011Motor is running reverse
010Motor is running reverse
000Motor is stopping
100Motor is running forward
 
Now if you do the sequence below the drive will stay in ready:
DI1 (forward)DI2 (reverse)DI5 (FW limit switch)Note
100Motor is running forward
101Motor is stopping
000Sensor goes back to low level
010Motor is running reverse
000Motor is stopping
100Drive stays in ready
 
The drive stays in ready as the behavior isn't coherent. The limit switch shouldn't have change of state, before reverse order.


 

Schneider Electric Nigeria

Attachment(s)
_9xx_20160921-Postioning by Sensors.pdf [120.4 KB]
ProgManual-Limit Switches and Positioning by Sensors.pdf [369.97 KB]
Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:
move-arrow-top