Search FAQs
Video: Can you use a standard CAT5 cable to connect the ATV630 process drive and the VW3A1111 remote keypad.
Issue:
Using a standard CAT5 cable to connect the ATV630 process drive and the VW3A1111 remote keypad.
Product Line:
ATV630 and ATV930 drive
Environment:
All
Cause:
Wants to connect a standard CAT5 cable to connect the VW3A1111 to the ATV61 drives HMI port.
Resolution:
Yes can you connect a standard CAT5 cable to the VW3A1111 keypad display.
You will need to remove the bottom rubber cover on the VW3A1111 keypad display. Once the rubber cover is pulled back you will see the RJ45 for attaching the CAT5 cable.
Using a standard CAT5 cable to connect the ATV630 process drive and the VW3A1111 remote keypad.
Product Line:
ATV630 and ATV930 drive
Environment:
All
Cause:
Wants to connect a standard CAT5 cable to connect the VW3A1111 to the ATV61 drives HMI port.
Resolution:
Yes can you connect a standard CAT5 cable to the VW3A1111 keypad display.
You will need to remove the bottom rubber cover on the VW3A1111 keypad display. Once the rubber cover is pulled back you will see the RJ45 for attaching the CAT5 cable.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: