Issue:
Implement Ethernet/IP explicit messaging in SoMachine?
Product Line:
SoMachine
Resolution:
Using the TM251MESE or the Ethernet version of the TM241 controller, with SoMachine V4.2, you can send and receive explicit messages by using function blocks EIPXM.Set_Attribute_Single and EIPXM.Get_Attribute_Single.
See attached screenshot from the help file of SoMachine.
Implement Ethernet/IP explicit messaging in SoMachine?
Product Line:
SoMachine
Resolution:
Using the TM251MESE or the Ethernet version of the TM241 controller, with SoMachine V4.2, you can send and receive explicit messages by using function blocks EIPXM.Set_Attribute_Single and EIPXM.Get_Attribute_Single.
See attached screenshot from the help file of SoMachine.