{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you protect the drive from users accessing menus on the ATV61 and ATV71 drive?
Issue:
Protect access of the ATV61/ATV71 menus.

Product Line:
Altivar 61, Altivar 71

Environment:
All

Cause:
Protection.

Resolution:
This function is available under 7.3.
You can either choose to protect or make invisible entire menus or select the parameters needed.

Schneider Electric Nigeria