Search FAQs
Video: How can I restore my Vista template diagram to the default configuration?
Issue:
The default vista diagram for a meter type has been edited and must be to restored it to its default configuration.
Product Line:
ION Enterprise 6.0
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment:
Vista
Cause:
If an edit is made to the template diagram, such as linking it to a specific node, that change will reflect across all diagrams for devices of that type. For example if a voltage measurement on the template diagram is linked to a specific node it will now only pull the voltage measurement from that device no matter which device of that type is being viewed.
Resolution:
The steps to restore the template diagram to the default state are covered in the video below.
The default vista diagram for a meter type has been edited and must be to restored it to its default configuration.
Product Line:
ION Enterprise 6.0
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment:
Vista
Cause:
If an edit is made to the template diagram, such as linking it to a specific node, that change will reflect across all diagrams for devices of that type. For example if a voltage measurement on the template diagram is linked to a specific node it will now only pull the voltage measurement from that device no matter which device of that type is being viewed.
Resolution:
The steps to restore the template diagram to the default state are covered in the video below.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: