{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the heat sink fan replacement part numbers for the ATV630, ATV930 and ATV660 Altivar Process Drives?

Issue:
What are the heat-sink fan part numbers for the Altivar Process Drives?

Product Line:
Altivar Process Drives (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drives

Cause:
Need part numbers to order or replace the fans

Resolution:

Open Style Products (Altivar 630/930 and Altivar 650/950)

img1


Enclosed Drive Systems (Altivar 660/960 and Altivar 680/980)
Fan Part Numbers & Quantity:

  • Size 1
    • 110kW - 160kW (125hp - 200hp)
    • Need 1 of each
      • VX5VPM001 - Fan Kit, Connection Cables
      • VX5VPM003 - Enclosure Door Fan
  • Size 2
    • 200kW - 315kW (250hp - 500hp)
    • Need 2 of each
      • VX5VPM001 - Fan Kit, Connection Cables
    • Need 1
      • VX5VPM003 - Enclosure Door Fan
  • Size 3
    • 400kW - 500kW (500hp - 600hp)
    • Need 3 of each
      • VX5VPM001 - Fan Kit, Connection Cables
    • Need 1
      • VX5VPM003 - Enclosure Door Fan
  • Size 4
    • 630kW (700hp)
    • Need 4 of each
      • VX5VPM001 - Fan Kit, Connection Cables
    • Need 1
      • VX5VPM003 - Enclosure Door Fan

Enclosed Drive Systems below size 110kW use the open style drives in the enclosure so for the fan part numbers use the table above.
For Example - ATV660D30T4N..... uses the ATV630D30N4 power converter so use the VX5VPS4001 for the fan part number.

Other Part Numbers for Enclosed Drive Systems to consider getting if replacing the fans maybe...

  • VX5XPM002 - DC-Supply for Fan
  • VX4XPMC1180N4 - Fan Supply Board
    • Quantity maybe different based on frame size. Drive will require 1 more fan supply board than the quantity of fan kits needed.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Attachment(s)
ATV630_IS_Fan_Size_1-2-3_EAV64373_02.pdf [4.99 MB]