{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATV630/930 have a built in time delay feature for digital inputs?
Issue:
Time delay feature for digital inputs in the ATV630/930

Product line:
Altivar Process ATV630 ATV930

Environment:
All models

Cause:
n/a

Resolution:
All of the digital inputs have an ON Delay setting range of 0-200msec.  The factory default is 0msec.
Under Complete settings -> Input/Output -> DI/DQ -> DIx Config, set DIx Delay to the desired time delay.

This delay setting works only as an ON delay, for DIx going active.  There is not a delay feature for OFF delay.

Schneider Electric Nigeria