{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert 8.2 - why can't I access the Rate Editor/Hierarchy Manager/Alarm Configuration from the Management Console?
Issue
PME is configured to use SSL and the HTTP binding is removed from IIS, the links from the Management Console to the web applications will no longer work.

Product Line
Power monitoring Expert 8.x

Environment
Management Console
Internet Explorer

Cause
Links in Management Console point to a HTTP location, which was deactivated, and cannot be changed.

The affected web applications are:
* Rate Editor
* Hierarchy Manager
* Alarm Configuration

Resolution

All of these web applications can be accessed from the Settings area of Web Applications in PME 8.2. Note that it is generally bad practice to access web applications directly from the server, and the links in the Management Console will be removed in a future PME release.

Schneider Electric Nigeria