{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does it fix for sv8.09 of the TCSESM connexium switches?
Question:
What does it fix for sv8.09 of the TCSESM connexium switches as there is no version history file on shoppingkiosk?

Answer:
One issue was to upgrade the CTick marking.  CTick is the Australian Communications Media Authority.  The marking signifies the device is compliant with their EMC requirements.

The second issue fixes an SNMPv3 vulnerability that may allow authentication bypass if specially crafted packets are used.

Schneider Electric Nigeria