{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert 8.2 - When first installed with ENM, the very first event in the PME EventLog2 table in ION_Data will be missed by ENM
FYI - In a new PME + ENM install, ENM will miss the very first record written to the EventLog2 table in the PME ION_Data database. This will only occur once, immediately after the software is installed, and the only event that will be missed by ENM is the very first record written to the PME EventLog2 table. From that point on, ENM will retrieve all subsequent PME events.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.