{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
latest firmware update for the TM168MODW
Issue

What is the latest firmware update for the TM168MODW?

Product line

M168


Resolution

The latest firmware update for the TM168MODW is attached. The procedure to upgrade the module is as follow:
1. Unzip the contents of this attachment to pc/laptop
2. Open DOS Window (cmd.exe)
3. Run UpdateCoPla.bat with parameter set to IP Address of MODW, e.g. C:>UpdateCoPla 192.168.1.52 4 If the # of bytes sent is equal to display hit space to continue, otherwise power cycle and repeat.

Schneider Electric Nigeria

Attachment(s)
V2.02.01.012-exe.zip [516.41 KB]