{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do we decode the Date of Manufacture (DOM) on the Magelis series of HMIs?
Issue:
Where on the label of the Magelis HMI can we find information regarding the date in which the unit was produced?

Product Line:
Magelis series of HMI, XBTG, XBTGT, HMIGTO, HMISTO, HMISTU, HMIGTU, HMIGK

Resolution:
On the back of a Magelis HMI, there is a sticker/label with the Date of Manufacture (DOM) on it. The code is typically 4 digits like this: 1533. For this particular example, it decodes as Year:2015, Week 33.

Therefore in general terms the date code is: YYWW where YY is the last two digits of the year and WW is the week number in that particular year.

Schneider Electric Nigeria