{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to fix an unexpected shutdown of the Magelis iPC?
An important CPU usage brings about a temperature elevation of the CPU.
When the temperature threshold is reached, in order to safe the material, the operating system shuts down the system.

By default, this temperature threshold is set to 95°C but it is possible to increase it to 105°C.
See the procedure in the attached document.

iPC offer:
- Standard references: HMIBMPxxx, HMIBMUxxx, HMIPSPxxx, HMIPEPxxx, HMIPSOxxx
- Configured references: HMIPCCU2xxx, HMIPCCP2xxx, HMIPCCS2xxx

Schneider Electric Nigeria

Attachment(s)
CPU_Shutdown_Temeperature.pdf [310.32 KB]