{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you run the ATV61 and ATV71 Drive without the HMI on the face of the drive?
Issue:
Can you run the ATV61 and ATV71 Drive without the HMI?

Product Line:
Altivar ATV61 and ATV71 drive

Environment:
All

Cause:
Wants to take off the HMI and still run the drive.

Resolution:
You can run the ATV61 and ATV71 drive without the HMI on the face of the drive as long as the drive is not programmed to be controlled with the HMI like wheel is the knob is the speed control or the start stop buttons are active.

Schneider Electric Nigeria