{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there an Add-on Profile available for ATV320 for Ethernet IP?
Issue:
Looking for a Add-on Profile for ATV320, for Ethernet IP?

Product Line:
ATV320, Altivar 320

Environment:
All

Cause:
NA

Resolution:
There is no dedicated Add-On Profile (AOP) available for the ATV320 series drive.
We only provide the EDS file to integrate the drive inside Rockwell PLCs.

Schneider Electric Nigeria