{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If we add MCC in Prisma P will it be type tested or not ?
1-Prisma P and Prisma G can be equipped with :

a-Circuit breaker type GV2+Series D and K contactors less or equal 40Ampere
b-Tesys U
c-Soft starters Altistart 01 types:
ATS01N103/106FT
ATS01N109/112FT
ATS01N206 to 212
ATS01N222 to 232
ATS01N230LY
ATS01N244LY
ATS01N244Q
ATS01N272LY
ATS01N285LY
ATS01N272Q
ATS01N285Q

2-Dedicated enclosures for MCC Prisma Plus Fixed or disconnectable-type switchboards,with maximum motor rating 37KW(D.O.L./2 speed/star delta) with 3 components (breaker +contactor+overload relay) OR maximum 15KW using the tesys U.(available Test certificate for Fixed type attached).
Please note that the fixed type can adapted for form 2b or 4a ,while disconnectable type is form2.Thanks to confirm with the product manager its commercialisation in the country.

N.B.Prisma doesn't comply with NEMA standard.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.