{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Have the Pedestal and Deadband been reversed on the Process Drives compared to the ATV61/71 drives?
Issue:
The Pedestal and Deadband appear to have been reversed on the Process Drives compared to the ATV61/71 drives.

Product Line:
ATV630, ATV930

Environment:
Pedestal and deadband

Cause:
n/a

Resolution:
Response from France:
We are aware about that and we are waiting for the solution.
Appears to be a problem on the keypad and SoMove.
Parameter BSP can have a setting of Standard, Pedestal, Deadband or Deadband 0 % :
When you see the Keypad: BSP can be standard , Deadband, pedestal or pedestal at 0%:
The term is inverted on keypad : Deadband should be Pedestal and pededstal /pedestal at 0% should Deadband/Deadband at 0%.
Same problem with SoMove:
The solution to set Pedestal like on ATV71, is to set Deadband on ATV6XX/ATV9xx.
We have asked for a solution on future softwares on the Keypad and SoMove.

Schneider Electric Nigeria