Search FAQs
What is Control Expert (formerly Unity Pro) "Student Simulation Only"?
Control Expert / Unity Pro version v12.0 and later offers a "Student Simulation Only" package.
It is dedicated to help students train and become familiar with Unity Pro engineering software.
“Student Simulation Only” allows simulation of applications for M580 (medium range CPU) and M340.
It supports limited features, and can only be used for student’s study and training purposes.
“Student Simulation Only” can only be used to develop an application that runs on Unity Pro PLC Simulator only.
It cannot connect to a real PLC, nor generate an application for a real PLC (Only Simulator).
An application developed with Control Expert/Unity Pro “Student Simulation Only” must not be opened or run with any standard version of Control Expert/Unity Pro.
Any other usage is strictly forbidden.
The software can be run for unlimited period of time: no registration is required.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: