Issue:
Can I check the part number, serial number, and other information on the ATV630 and ATV930 process drive using the keypad?
Product Line:
ATV600 and ATV900 series drives
Environment:
All models, All serial numbers
Cause:
Information not clear in current literature.
Resolution:
First access the Main Menu by pushing the button shaped like a House.
Then press the blank button below the left hand side of the display (display shows Drive ID directly above this button.)
This will give you access to the Drive Identification menu.
The values displayed are:
Can I check the part number, serial number, and other information on the ATV630 and ATV930 process drive using the keypad?
Product Line:
ATV600 and ATV900 series drives
Environment:
All models, All serial numbers
Cause:
Information not clear in current literature.
Resolution:
First access the Main Menu by pushing the button shaped like a House.
Then press the blank button below the left hand side of the display (display shows Drive ID directly above this button.)
This will give you access to the Drive Identification menu.
The values displayed are:
- DEVN - This is the device number. Example: ATV630U07M3
- kW/HP of the product
- Voltage of the product
- Application Version
- MC (Motor Control) Version
- Ethernet Version
- CPLD Version
- PWR Version
- Serial number (consists of the next 2 lines displayed)
- Product Version
- Option 1 will display the information of the option card installed in slot A (if one is present) including part number, version number and serial number
- Option 2 will display the information of the option card installed in slot B (if one is present) including part number, version number and serial number
- Graphic Display terminal will display the Version and serial number of the graphic keypad