{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the maximum allowable temperature on the terminals of a Masterpact NW ACB?

Masterpact NW ACBs comply with IEC 60947-2. Temperature rise tests for Masterpact NW ACBs are specified in standard IEC 60947-2. Please find attached a declaration of conformity illustrating the maximum allowable temperature on the terminals of the Masterpact NW ACB.

Schneider Electric Nigeria

Attachment(s)

Masterpact NW Max Connection Temperature.pdfMasterpact NW Max Connection Temperature.pdf [24.1 KB]